DIO#.FILTER
Description
Gets or sets the digital input filter when specified channel is configured as a digital input (see DIO#.DIR). The digital filter blocks input changes (rising or falling edges) until the minimum pulse width is exceeded. The +/- tolerance listed is the sample period (uncertainty) of the filter.
| Value | Description | Min Pulse Width | Typical Use |
|---|---|---|---|
| 0 | Unfiltered | >40ns | RS485 inputs |
| 4 | Ultra fast |
>240ns +/- 40ns |
Fast Optos |
| 1 | Fast |
>10.24 µs +/- 0.64 µs |
Fast Optos |
| 2 | Standard |
>163µs +/- 10.24µs |
Slow Optos |
| 3 | Slow |
>2.62ms +/- 0.16384ms |
Mechanical switch |
Usage
When DIO#.DIR = 0 (input) then the corresponding DIO#.FILTER can be set to adjust the filter of the input value.
Code
--> DI01.DIR 0 --> DIO1.FILTER 0 --> DIO1.FILTER 1
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 4 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DIO1.FILTER |
368ah |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO2.FILTER |
368bh |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO3.FILTER |
368ch |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO4.FILTER |
368dh |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO5.FILTER |
368eh |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO6.FILTER |
368fh |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
22250 |
1 |
22250 (0x56ea) |
DIO1.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
22251 |
1 |
22251 (0x56eb) |
DIO2.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
22252 |
1 |
22252 (0x56ec) |
DIO3.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
22253 |
1 |
22253 (0x56ed) |
DIO4.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
22254 |
1 |
22254 (0x56ee) |
DIO5.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
22255 |
1 |
22255 (0x56ef) |
DIO6.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DIO1.FILTER |
22250 |
Unsigned8 |
Read/Write |
- |
|
DIO2.FILTER |
22251 |
Unsigned8 |
Read/Write |
- |
|
DIO3.FILTER |
22252 |
Unsigned8 |
Read/Write |
- |
|
DIO4.FILTER |
22253 |
Unsigned8 |
Read/Write |
- |
|
DIO5.FILTER |
22254 |
Unsigned8 |
Read/Write |
- |
|
DIO6.FILTER |
22255 |
Unsigned8 |
Read/Write |
- |